Radical Automation: Radwell International's Blog

The Basics of an Industrial Circuit Breaker

Written by Radwell International | Jun 12, 2024 12:00:00 PM

From home electrical systems to advanced industrial circuits, circuit breakers protect power systems from electrical power overloads, ground faults, arc faults, and other scenarios where electricity could pose a safety risk to people and property. In the case of a fault, circuit breakers interrupt the flow of electricity, limiting the energy available to cause damage. 

How does a Circuit Breaker work?

The most common type of circuit breaker contains an electromagnet and a movable armature with an electrical contactor at the end. The arm is connected to a spring or other actuator, and the arm contactor makes contact with a stationary contactor inside the breaker, completing the circuit and allowing electricity to flow. When a problem occurs, the actuator forces the contactors apart, stopping the flow of electricity. The primary factors to consider when choosing a circuit breaker are the voltage (electrical power standing still), current (voltage moving through a conductor over time), and where the breaker will be installed.

Types of Industrial Circuit Breakers

Miniature circuit breakers (MCB):

MCBs are commonly used in low voltage applications such as 24 V DC or 125 V AC circuits. These devices have ratings ranging from 0.5 A to 30 A. Miniature breakers can be found in automobiles, small appliances, and office equipment, among other applications. They typically have a generic mounting system, such as a DIN rail, or are housed inside a control panel.

Molded Case Circuit Breakers (MCCB):

MCCBs are the most common type of circuit breaker. They have higher current-carrying capacity than miniature breakers, ranging from 3 A to more than 4,000 A. In these devices, a thermal-magnetic trip unit typically opens the circuit breaker when the electrical current exceeds the breaker’s rating, causing a metal sensor to actuate or turn on. Molded case circuit breakers are widely used in residential and commercial applications.

Insulated Case Circuit Breakers (ICCB):

ICCBs are similar to molded case circuit breakers. Still, unlike MCCBs, insulated case breakers often use an electronic circuit to monitor electrical current and stored energy mechanics that can be charged by manipulating a charging handle. They have the functionality of a larger, more capable iron or air-frame circuit breaker or a low-voltage power breaker with a molded plastic frame instead of a metal frame. These breakers can be regularly reconditioned and returned to service.

Air Circuit Breaker (ACB):

ACBs move exclusively beyond low voltage (0-0.6 kV) to medium-voltage power distribution (0.6 kV-33kV). Unlike the breakers discussed earlier, an ACB’s metal frame supports internal components rather than providing an insulating layer (made of plastic in the low-voltage breakers described above). While MCBs and MCCBs are regularly used near the devices they protect, with their higher load capabilities, ACBs can act as disconnect switches for industry and other power-hungry applications. ACBs generally have an upper limit of 15 kV but are regularly replaced by more reliable vacuum circuit breakers.

Vacuum Circuit Breaker (VCB):

A VCB has a vacuum interrupter, sometimes called a vacuum bottle, and a spring-loaded moving contact. A vacuum interrupter is made of two electrodes in a vacuum chamber. The arc that forms when the contacts open is extinguished in the vacuum.

Gas Circuit Breaker (SF6):

While overcurrent protection from a VCB can be degraded by metal molecules floating inside the chamber, reducing the ability of the vacuum to quench an electrical arc, gas circuit breakers typically use a dielectric insulating gas such as sulfur hexafluoride (SF6) to help cool down and quickly extinguish an arc. Advantages include low maintenance, lower operating noise, and no emission of hot gases. Gas circuit breakers are commonly used for high-voltage applications with utility-grade equipment ranging from 35 kV to 500 kV. An advantage of this type of circuit breaker is that it can be used to make and break relatively large currents under normal and fault conditions. Also, it has low maintenance costs and a longer life than an ACB. VCBs are primarily used in power generation facilities and heavy industrial applications.

 

Connection Types in Industrial Circuit Breakers

A circuit breaker has multiple connection types:

Plug-In:

Plug-in circuit breakers connect to the bus bar using plugs on either side of the breaker, allowing for easy installation and removing a breaker. Popular plug-in breakers include the Square D I-line system, although different manufacturers utilize different plug-in systems.

Bolt-On:

Bolt-On breakers connect to the bus bar using threaded studs. These studs are placed through holes in the bus bar and tightened with nuts and washers. This connection is often the least expensive and most secure. However, installing, replacing, or temporarily removing a bolt-on breaker can be difficult.

Feed-Through:

Feed-Through circuit breakers have lugs on both sides that connect cables to the breaker. They are sometimes called cable-in and cable-out breakers because cables are utilized to send power to and from (For example, line/load) the breaker.

Pole Numbers of Industrial Circuit Breakers

The number of poles determines how many separate circuits can be simultaneously protected by a circuit breaker.

What is a One Pole Circuit Breaker?

One Pole Circuit Breakers are typically used in fans, lighting equipment and single-phase applications. This is the most common configuration found in households.

What is a Two Pole Circuit Breaker?

Two Pole Circuit Breakers are used when connecting to multiple phases of a single or 3 phase circuit. This configuration is commonly used in homes for 240 V circuits, such as dryers and air conditioners.

What is a Three Pole Circuit Breaker?

Three Pole Circuit Breakers are used in 3-phase applications. This is commonly used to feed 3-phase subpanels or 3-phase-rated equipment such as large motors.

What is a Four Pole Circuit Breaker?

Four Pole Circuit Breakers are used in 3-phase systems with an extra fourth pole to protect the neutral circuit within the system. This is commonly used in data centers and scenarios requiring a high degree of coordination or protection of sensitive equipment.

Important terms related to circuit breakers:

Volts vs. Current

Voltage is electricity at rest and is measured in volts, while a current is an electrical charge in motion over time and is measured in amps. The difference between the high and low points in an electrical field defines the potential or voltage present. In alternating current (AC) systems, the voltage changes from negative to positive and back to positive in a continuous wave. Direct current (DC) systems maintain a consistent positive or negative voltage.

AMPS

Amperes are the units used to measure current or an electrical charge in motion. When describing voltage, current, and resistance, a common analogy is a water tank. In this analogy, the charge is represented by the water amount, the water pressure represents voltage, and the water flow represents current.

AIC Rating

Ampere interrupting capacity (AIC) is the maximum current a circuit breaker has been designed to interrupt, protecting downstream equipment and people. AIC is measured in amps at a particular voltage. For example, 18 kA @480 V or 65 kA @480 V)

Circuit Breaker Accessories

Various circuit breaker accessories come into play to enable features such as remote indication and automatic operation. Here are a few examples:

Auxiliary Switch:

The auxiliary switch indicates the breaker’s present condition: open or closed. The switch commonly defines operational states, such as NO (normally open), NC (normally closed), or a combination.

Closed Switch:

A closed switch indicates whether the circuit is closed and electricity can flow.

Bell Alarm:

A bell alarm provides a remote indication that a circuit breaker has tripped due to an electrical fault.

Motor/Electric Operator:

Circuit breaker springs can be very powerful. In some cases, a motor electric operator helps compress a spring so it can open, moving the electrical contacts away from each other and interrupting electrical flow in the case of a fault. It is also used to charge a circuit breaker remotely without physical access.

Shunt Trip:

A shunt trip remotely trips a breaker when voltage is applied. It is used to safely trip a breaker via a remote panel or to automatically trip it using another device (such as another circuit breaker).

 

Learn how Radwell can help your business with automation, electrical and MRO parts & expert services.