It’s been over 50 years since the birth of the Programmable Logic Controller. We look back at the history of the PLC and how replacing hard wired relay systems changed the world of manufacturing.
It was the year 1964 when a young cunning engineer, Dick Morley, was unemployed, had a new baby, a mortgage to pay and only $1,000 in the bank. Morley had previously worked a desk job designing atomic bombs, airplanes and communication systems performing the duties he was instructed to do.
Morley did not enjoy his job, and, at that time, he had no plans in the pipeline to create such an influential piece of automated equipment. After finding his passion for skiing, Morely quit his job and focused on his hobby which eventually lead him to engineering ideas.
Morley eventually opened up his own professional consulting firm with friend Geogre Schwenk under the name ‘Bedford Associates’’ located in Bedford, Massachusetts, USA. Morley and Schwenk worked with local machine tool firms to help them evolve into the new, solid-state manufacturing sphere. Unfortunately, as his firm progressed, he began to notice that each project he worked on was practically the same; the manufacturing industry was using similar minicomputers and Morley found himself bored.
With his creativity and his engineering motive to ‘make things work’, Morley started to wonder if he could invent a controller which could automate industrial process with multiple input/output arrangements in real time. This would alternately replace the likes of hardwired relay control systems.
Morley started to draft up a proposal, but it wasn’t until New Year’s Day that Morley put his ideas onto paper whilst nursing a hangover. On that day, he managed to map out the functions of a Programmable Logic Controller which would later revolutionize the way engineers operated production sites.
The PLC was designed to be robust and to withstand harsh conditions such as severe heat, cold and moisture. The PLC did not have to be placed in a sealed cabinet as the unit transferred air out through large metal fins so no dirty air modules got inside the electronics.
With financial backing, in October 1968 a new company was formed called Modicon, now
known as Schneider Electric. At this point, Morely, Greenberth, Landau and Boissevain were not the only engineers who wanted a replacement to the relay systems; Bill Stone at GM Hydramatic also desired a single unit that was able to control a production assembly line. The programmable logic controller was in demand.
Today’s production lines
The Programmable Logic Controller has been an integral part of automation and industrial process control for decades, with a varied range of applications it can control chemical plants, food processing sites environmental systems and even a simple light. The PLC can read signals from various sensors, keyboards, switches and input devices. Output devices include motors and solenoid valves that complete the full automated system. The PLC can run both dc and ac input/output modules, changing voltage, direction, speed and set times; the relay can only be switched on and off one direct, unable to change voltage and speed.
Dick Morley generated a revolution in the automation industry, compacted a clever CPU into a unit and took away the element of hard wiring relay systems that provided engineers with many technical difficulties. PLCs continue to be advanced technology that can be developed just like consumer electronics.
To learn more about Radwell International and how we can support your PLC needs