What is an Actuator?
An actuator is the main component of a mechanical device that allows the device to move. This movement can be in two forms, one being linear the other being rotary. Linear movement means it can move back and forth on a set path in a straight motion. Rotary movement means movement in a rotational fashion. These two types of movement allow for actuators to be broken down into a linear actuator and a rotary actuator.
Rotary actuators are not only different from linear actuators through the type of movement they produce, but also due to them not being on a set path. A rotary actuator can keep rotating in the same direction for as long as necessary. This type of continuous rotational movement allows for rotary actuators to power heavy machinery. It aids heavy machinery in mixing, dumping, screw clamping, turning over, and providing constant tension.
There are additional types of actuators as well. Linear and rotary will always be at the core of actuators depending on the type of movement they provide. But there are three other types of actuators that vary based on how the control signal and power source is provided. The three main forms of control signals and source of energy are; electrical current, hydraulic fluid pressure, or pneumatic pressure. This results in electric actuators, hydraulic actuators, and pneumatic actuators. All of these types of actuators are capable of being linear or rotary.
When a large amount of force is required, hydraulic actuators are the correct choice and this is due to the fluids powering hydraulic actuators, which are impossible to compress. This incompressible ability from hydraulic actuators allows for them to exert a large amount of force as well as its ability to constantly hold that force or toque. Consisting of a piston inside a hollow cylinder, fluid is sent in from an external valve. That fluid sent in from the external valve moves the piston due to the created pressure by the overwhelming fluids. Hydraulic actuators have one main downfall. Unlike the cleanliness of an electric actuator, the hydraulic fluid is the complete opposite. It will have leaks and the loss of this fluid will not only create a mess, it will lead to less efficiency as well.
Actuators come in many different forms that are suitable for different needs. If the need is precision, electric actuators are the correct choice. If a high force and torque are needed, hydraulic actuators would be the go-to. Simplicity would be electric actuators. Each of the different types of actuators has their advantages and disadvantages. It all comes down to choosing an actuator that is appropriate for the needs of the mechanical device it will be a part of.
To learn about how Radwell can assist you with your product and repair needs
To learn more about Radwell International