Just as with medical x-rays that people receive to look at broken bones, our x-ray unit is used to see within the bodies and cases of equipment and parts. We utilize the x-ray machine to look inside objects that would normally defy inspection, such as the inner traces of printed circuit boards (PCBs), internal connections of individual electronic components, and integrated circuits (ICs). We also use the x-ray machine to help identify unknown components that may be “house marked” with a proprietary part number or that bear no identification at all. Assisting in the replacement of special ICs known as BGA (Ball Grid Array) is another task that the X-Ray machine is used for.
Used routinely as a means to identify traces within a circuit board, the x-ray machine helps identify the connections between the components that make up the circuits. This is important because when boards that are old, obsolete or unique get damaged, there is very often no way to replace them. They must be repaired and being able to see and follow the traces within the circuit board allows repair technicians to identify damaged areas. It also helps repair technicians see where alternate connections can be made to complete the circuit during the repair process.
Sometimes, performing “engineering” modifications is the only way to keep damaged equipment operating. This is an incredible asset to our customers who are using older equipment. If an application or machine couldn’t be repaired, it would have to be replaced. This can be incredibly costly and might even pose a hardship for the company in question. Being able to utilize x-ray technology to help assist in accomplishing these types of repairs is invaluable to our customers.
In some cases, we can determine the function of a component merely by identifying
When repairing PCBs with special ICs known as “Ball Grid Array” ICs, the x-ray machine is necessary for inspection of the completed work. BGA ICs utilize small balls of solder attached to the very bottom of the IC itself. Because the construction of these parts puts all the connections underneath the component, a human cannot solder or de-solder these connections. For this reason a special machine is needed
We have the capability to provide our industrial automation clients with a high level of service. Utilizing x-ray technology is yet another valuable tool in our extensive tool box of solutions for our clients at Radwell International.
-Mike Thompson for Radwell International