Radical Automation: Radwell International's Blog

Variable Frequency Drives: Proper Maintenance Matters

Written by Julie Basello | Jun 21, 2023 11:45:00 AM

Variable Frequency Drives (VFDs) are electronic devices that are used to control the speed and torque of an AC electric motor. They work by adjusting the frequency and voltage of the electrical power supplied to the motor, which in turn changes the motor's speed and torque.

Before we review recommended maintenance for VFD’s, here’s a brief overview of how VFDs operate:

Rectification: The incoming AC voltage is first converted to DC voltage through a rectifier circuit.

Filtering: The DC voltage is then filtered to smooth out any fluctuations or noise in the signal.

Inversion: The filtered DC voltage is then converted back to AC voltage through an inverter circuit. The inverter circuit produces a variable frequency and voltage output that is used to control the motor.

Control: The VFD's control circuitry monitors the motor's speed and adjusts the frequency and voltage of the output to maintain the desired speed and torque.

Feedback: The VFD can also receive feedback from sensors that measure the motor's speed, current, and temperature, allowing it to make real-time adjustments to the output.

Overall, VFDs offer precise control over motor speed and torque, which can lead to energy savings, increased efficiency, and longer equipment life. They are commonly used in industrial applications such as pumps, fans, and conveyors, as well as in HVAC systems and other commercial and residential applications.

 

How do VFDs make machinery operate? Here's how VFDs make machinery move:

  • AC electric power is supplied to the VFD, which then converts it to DC voltage through a rectifier circuit.
  • The DC voltage is then filtered to remove any noise or fluctuations in the signal.
  • The filtered DC voltage is then inverted back to AC voltage through an inverter circuit. The inverter circuit produces a variable frequency and voltage output that is used to control the motor.
  • The motor is connected to the VFD's output, and the VFD's control circuitry monitors the motor's speed and adjusts the frequency and voltage of the output to maintain the desired speed and torque.
  • As the motor's speed and torque output changes, it drives the machinery connected to it. For example, a conveyor belt or a pump may be connected to the motor's output, and as the motor speeds up or slows down, so does the conveyor belt or pump.

Variable Frequency Drives require proper maintenance to ensure their continued reliability and performance. Here are some tips to help keep VFDs in good repair:

Regular inspection: Regular inspection of VFDs is essential to identify and address any issues before they become major problems. Inspect the VFDs for signs of overheating, loose connections, and damaged or worn components.

Preventive maintenance: Develop and follow a preventive maintenance plan for VFDs, which includes regular cleaning, lubrication, and replacement of worn or damaged components. This helps to extend the life of the VFD and prevent failures.

Proper installation: Proper installation of VFDs is essential for their reliable operation. Ensure that VFDs are installed according to the manufacturer's specifications, and that they are installed in a clean and dry environment.

Use the right VFD for the job: Ensure that the VFD is properly sized and rated for the motor and application it is controlling. Using the wrong VFD can cause it to fail prematurely or operate inefficiently.

Proper grounding: Proper grounding is important to prevent electrical interference and ensure safe operation of VFDs. Follow the manufacturer's instructions for grounding the VFD.

Keep VFDs clean and cool: Dirt, dust, and other contaminants can cause VFDs to overheat and fail. Keep the VFDs clean and ensure that they are properly ventilated to dissipate heat.

Regular calibration: Regular calibration of VFDs is essential to ensure their continued accuracy and reliability. Follow the manufacturer's instructions for calibration.

 

By following these tips, you can help to keep VFDs in good repair, ensuring their continued reliability and performance.

 

 

********

To learn more about Radwell’s Repair and Maintenance Assistance for your VFDs