In the industrial, engineering, manufacturing and scientific industries, valves serve multiple purposes. Their main purpose, however, is to control a specific medium flow through a system. Typically, valves may be used to start, stop, or throttle the flow to ensure safe and efficient operation of the process. Valves come in many different types and arguably the most dependable, cost-effective, and consistent control at relatively low flow rates are proportional control valves.
The three forms of output being; direction, pressure, or flow. These three forms of output result in three forms of proportional control valves. Proportional flow control valve, proportional pressure control valve, proportional directional control valve.
A proportional flow control valve controls the regulation of the amount of medium passing through a hydraulic system. With the use of internal positional feedback to indicate the position of the valve spool when a signal is provided. The feedback helps the amplifier determine the position of the spool and allows the amplifier to provide proper voltage, so the spool moves to the proper position inside the valve. This position of the valve spool is very important to controlling fluid flow.
Proportional pressure control valves allow for machines to properly control or maintain the pressure applied or the pressure relieved. This action is undertaken solely by changing throttling cross-sections with the aid of mechanical, electrical, or hydraulic adjustment movements. Relieving the pressure with a proportional valve is used when a fluid system has too much pressure. With the design to open gradually as pressure increases or close when the system falls below the set pressure.
Each one of these can be found on different applications. Proportional flow control valves are typically used for paint spray systems, filling systems, fluid dispense, or tank flow control. Proportional pressure control valves are used for pneumatic breaking, air bearing, or blow molding. They are also applied to generate a proportional force for spot welding, web/paper tension or clamping. Proportional directional control valves are primarily used to control the direction of flow between the components of a pneumatic circuit.
Each one of these types of proportional control valves perform different outputs. But each one has similar factors. One being proportional valve coils are arguably their most important feature. Operating on dc current and varying voltages, this allows the valves to produce a varying force to shift the spool. Theses coils normally demand an electrical input that is much stronger then the general electrical power provided. This results in the input current needing to be amplified. This function can be fulfilled by an amplifier card being mounted on the valve, commonly termed OBE (On Board Electronics).
Every proportional control valve, whether it is directional, flow, or pressure. Are designed with the thought to equalize the input flow of hydraulic fluid to match the output exactly. Due to their electronic signals ability to match the output exactly, they would be ideal for systems that need precise performance in variable pressure and flow applications.
Controlling flow is a key part of many industries. If it’s gas, air, steam, or any form of fluid, valves will play an important role in controlling those mediums. Proportional valves are just one of many valves that can benefit a company. If the pressure and flow control of machinery needs to be consistent proportional control valves can deliver.
To learn more about how Radwell can assist you with your valve repair and replacement needs