Controlling the flow and pressure of liquids and gases is an important part of many industries. Industrial, engineering, and manufacturing facilities rely on this capability. The main component that allows them the ability to do so are valves. Valves can vary in size, design, function and operation. But all have the purpose to control flow and pressure of liquids and gases. One of the most common and frequently used valves are solenoid valves.
Solenoid valves are used to regulate movement of gas or liquid in a system. They are tasked with the shutting off, releasing, dosing, distributing or even mixing fluids. Therefore, they are used wherever fluid flow must be controlled automatically. How they operate is by controlling the flow of the liquids or gases in a positive, full-closed or fully-open mode. The function involves either opening or closing an orifice in a valve body, which either allows or prevents flow through the valve. A plunger opens or closes the orifice by raising or lowering within a sleeve tube by energizing the coil.
Both types of solenoid valves consist of two basic parts; the solenoid attachment and the actual valve. Depending upon how many openings the valve has, a direct acting or pilot operate solenoid valve can be further broken down into a two-way valve, three-way valve, or four-way valve.
A two-way valve is the most basic solenoid valve. Referred to as a two-way valve due to having one inlet port and one outlet port. The two-way valve is used to either allow fluid flow in or to shut off the fluid flow. Depending upon how it is used, it can be specified as either “normally open” or “normally closed” in its operation. With a normally open valve, the valve remains open until some type of current is applied to close the valve. A normally closed works in the opposite fashion, remaining closed until a power source causes its open.
Four-way valves can have four or more port connections. Four-way valves are commonly used with a dual acting cylinder or actuator. In this version, half of the port connections supply pressure, and the remaining connections provide exhaust pressure. This provides a positive two directional action. They can be used instead of positioners to provide on/off operation of double-acting valves.
Many industries use solenoid valves for different applications, but all perform a similar function which is regulating the movement of some form of medium. Whether it is water, air, gas, oil, or even steam, solenoid valves aid in many industrial applications.
For information on how Radwell International can help you with your solenoid valve needs and repairs