Radical Automation: Radwell International's Blog

A Comprehensive Guide: Robotics for Beginners

Written by Radwell International | Jan 24, 2024 12:45:00 PM

Robotics technology is revolutionizing industries by automating processes, improving efficiency, and enhancing productivity. Understanding robotics technology is crucial for businesses and individuals alike, as it opens up new possibilities for innovation and growth. Since the field is evolving rapidly, acquiring knowledge about robotics enables individuals to stay competitive and adapt to the changing technological landscape. The purpose of this comprehensive guide is to provide readers with a detailed understanding of robotics technology. It aims to explain the principles, components, and applications of robots, as well as the factors to consider when choosing the right robot for a specific task. By exploring the world of robotics, readers can gain insights into this rapidly changing field and make informed decisions regarding the implementation of robots in various industries.

 

WHAT IS ROBOTICS TECHNOLOGY?

Robotics technology involves the design, development, and implementation of robots to perform tasks autonomously or under human guidance. Robots are mechanical devices equipped with various components and programmed to carry out specific operations. They can be designed for a wide range of applications, from industrial manufacturing to healthcare and exploration.

 

ROBOTIC COMPONENTS

 

MANIPULATOR (ROBOT ARM)

The manipulator, also known as the robot arm, is a crucial component of a robot. It consists of multiple joints connected by links, mimicking the human arm’s structure. The manipulator allows the robot to manipulate objects and perform tasks with precision and dexterity.

END OF ARM TOOLING (EOAT)

The EoAT, end effector, gripper, or tooling is the part of the robot that interacts with the environment or the object being manipulated. Grippers are commonly used end effectors that enable robots to grasp and handle objects. Other types of end effectors include welding tools, suction cups, and cutting devices.

SENSORS (VISION, PROXIMITY, FORCE)

Sensors play a vital role in robotics by providing robots with the ability to perceive and interact with their surroundings. Vision systems, such as cameras and depth sensors, enable robots to capture and process visual information. Proximity sensors help robots detect the presence or proximity of objects, while force sensors provide feedback on the forces exerted during interactions.

CONTROLLER AND PROGRAMMING INTERFACE

The controller is the brain of the robot, responsible for interpreting commands and coordinating the robot’s actions. It receives input from sensors, processes the data, and generates control signals for the robot’s actuators. The programming interface allows users to interact with the robot, either through a teach pendant or programming software, to program and control its behavior.

TYPES OF ROBOTS

Robots come in many different shapes and sizes, but there are six main types that are most commonly used. These are articulated robots, cobots, autonomous mobile robots (AMRs), automated guided vehicles (AGVs), humanoids, and hybrid robots.

ARTICULATED ROBOTS

Articulated robots are the most common type of industrial robot. They have a mechanical arm that resembles a human arm, and they are used for a variety of tasks, such as welding, painting, and assembly.

AUTOMATED GUIDED VEHICLES (AGVS)

AGVs are similar to AMRs, but they are guided by a pre-programmed path. They are often used in factories to transport materials between different workstations.

AUTONOMOUS MOBILE ROBOTS (AMRS)

AMRs are self-driving robots that can navigate their environment without human intervention. They are often used in warehouses and other large facilities to transport goods and materials.

COLLABORATIVE ROBOTS (COBOTS)

Cobots are robots that are designed to work safely alongside humans. They are often used in manufacturing environments, where they can collaborate with humans to perform tasks. Cobots are typically smaller and lighter than traditional industrial robots, and they have features that make them less likely to injure humans, such as having force and speed limits, as well as soft edges.

HYBRID ROBOTS

Hybrids are robots that combine the features of two or more of the other types of robots. For example, a hybrid robot might combine an AMR that can navigate its environment autonomously with a cobot for picking items from shelving.

HUMANOIDS

Humanoids are robots that are designed to look and move like humans. They are still in the early stages of development, but they have the potential to be used in a variety of applications, such as customer service and healthcare.

 

COMMON APPLICATIONS & INDUSTRIES WHERE ROBOTS ARE USED

Robotics technology finds applications in a wide range of industries. In manufacturing, robots are employed for tasks such as assembly, welding, and material handling, leading to increased efficiency and precision. In healthcare, robots assist in surgery, rehabilitation, and patient care. Robots also play significant roles in logistics and transportation, agriculture, construction, and exploration, among other fields.

 

ADVANTAGES & DISADVANTAGES OF ROBOTICS TECHNOLOGY

Robotics technology offers numerous advantages, including increased productivity, improved quality and precision, reduced labor costs, and enhanced safety in hazardous environments. Robots can perform repetitive tasks tirelessly and with consistent accuracy, leading to higher production rates. They can also work in environments that are dangerous or inaccessible to humans. However, robotics technology also presents challenges, such as high initial costs, and the need for skilled technicians. It is important to carefully evaluate the advantages and disadvantages before implementing robots in any given context.

 

HOW ROBOTICS TECHNOLOGY WORKS

 

BASIC PRINCIPLES OF ROBOT OPERATION

Robots operate based on three fundamental principles: perception, decision-making, and action. Perception involves gathering information about the environment through sensors. Decision-making refers to the robot’s ability to process the acquired information and determine the appropriate actions. Finally, action involves the physical movements performed by the robot’s actuators to carry out the desired tasks. transportation, agriculture, construction, and exploration, among other fields

 

ROBOT KINEMATICS AND MOTION CONTROL

Degrees of Freedom

Degrees of freedom (DOF) refers to the number of independent parameters that define a robot’s motion. A robot’s DOF determines its flexibility and range of movements. For example, a robot arm with six DOF can move in six different directions.

Joint & Cartesian Coordinate Systems

Robots can be controlled using joint or Cartesian coordinate systems. Joint coordinates define the positions of individual joints, while Cartesian coordinates describe the robot’s position and orientation in the workspace. Both coordinate systems have their advantages and are used depending on the application requirements

Forward & Inverse Kinematics

Forward kinematics involves determining the robot’s end effector position and orientation based on the joint angles. Inverse kinematics, on the other hand, calculates the joint angles required to achieve a desired end effector position and orientation. These kinematic calculations are crucial for controlling the robot’s movements accurately.

 

SENSING AND PERCEPTION PAYLOAD AND REACH REQUIREMENTS

Vision Systems & Image Processing

Vision systems equipped with cameras and image processing algorithms enable robots to perceive the visual information from their surroundings. This allows robots to detect objects, recognize patterns, and perform tasks that require visual feedback.

Object Detection & Recognition

Object detection and recognition algorithms enable robots to identify and locate specific objects within their environment. This capability is essential for tasks such as picking and placing objects or navigating through complex environments.

Force Sensing & Feedback Control

Force sensing enables robots to measure the forces exerted during interactions with objects or the environment. This feedback is used to adjust the robot’s actions, ensuring safe and precise operations. Force control allows robots to perform tasks that require delicate manipulation or contact force regulation.

 

ROBOT PROGRAMMING AND CONTROL

Programming languages (e.g., teach pendant, prog. software)

Robot programming can be performed using various languages and interfaces. Teach pendants provide a user-friendly interface that allows operators to manually program robots by demonstrating the desired motions. Programming software offers more advanced capabilities, including the ability to write scripts or use graphical programming languages.

Control modes (e.g., position, velocity, force)

Robots can be controlled in different modes, such as position, velocity, or force control. Position control ensures that the robot moves precisely to specified positions. Velocity control enables the robot to move at a specified speed. Force control allows the robot to maintain a specific force during interactions.

Motion planning and collision avoidance

Motion planning involves generating a sequence of robot motions to accomplish a task efficiently. Collision avoidance algorithms ensure that the robot avoids obstacles and other objects in its path. These capabilities are crucial for safe and optimal robot operations.

 

END EFFECTOR AND TOOLING COMPATIBILITY

GRIPPER TYPE AND GRIPPING FORCE

Different gripper types, such as parallel, vacuum, or robotic fingers, offer varying capabilities for object manipulation. Gripping force is also a crucial consideration, as it determines the robot’s ability to grasp objects securely. The gripper should be compatible with the objects and tasks involved.

TOOL CHANGING CAPABILITIES

Some applications require the ability to change end effectors or tools to perform different tasks. It is important to choose a robot that supports tool changing mechanisms to maximize versatility and flexibility in operations.

 

ROBOT CONTROL AND PROGRAMMING CAPABILITIES

USER INTERFACE AND PROGRAMMING SIMPLICITY

The robot’s user interface should be intuitive and easy to use. It should provide convenient programming options that match the user’s expertise and requirements. Simple programming interfaces enable quick setup and reconfiguration of robot tasks.

INTEGRATION WITH EXISTING SYSTEMS AND SOFTWARE

Compatibility with existing systems, such as manufacturing execution systems (MES) or computer-aided design (CAD) software, is essential for seamless integration. The robot’s control and programming capabilities should align with the existing infrastructure to streamline operations.

 

SAFETY FEATURES AND COLLABORATIVE CAPABILITIES

SAFETY STANDARDS COMPLIANCE (E.G., ISO 10218, ISO/TS 15066)

Ensuring the safety of operators and other personnel working alongside robots is of utmost importance. Compliance with safety standards, such as ISO 10218 for industrial robots and ISO/TS 15066 for collaborative robots, ensures that the robot meets the necessary safety requirements.

COLLABORATIVE ROBOT OPTIONS FOR HUMAN-ROBOT INTERACTION

Collaborative robots, or cobots, are specifically designed to work safely alongside humans. These robots have built-in safety features, such as force sensing or speed limitations, to prevent accidents and enable human-robot collaboration. Considering the collaborative capabilities is crucial for applications where humans and robots need to work together.

 

ENVIRONMENTAL CONSIDERATIONS

OPERATING ENVIRONMENT (E.G., TEMPERATURE, HUMIDITY)

The operating environment plays a significant role in choosing the right robot. Factors such as temperature, humidity, or the presence of dust and debris can affect the robot’s performance and longevity. It is important to select a robot that can operate reliably in the specific environmental conditions.

PROTECTION AGAINST DUST, WATER, AND OTHER CONTAMINANTS

Depending on the application, the robot may require protection against dust, water, or other contaminants. Robots with appropriate IP (Ingress Protection) ratings provide the necessary safeguards for reliable operation in challenging environments.

 

COST CONSIDERATIONS

INITIAL PURCHASE COST

The initial cost of acquiring a robot includes the cost of the robot itself, as well as any additional equipment or accessories required for its operation. It is important to consider budget constraints and evaluate the long-term benefits of the investment.

OPERATING AND MAINTENANCE COSTS

Operating and maintenance costs include factors such as energy consumption, preventive maintenance, and potential repairs. It is important to assess these costs to understand the overall financial implications of implementing a robot.

RETURN ON INVESTMENT AND PRODUCTIVITY GAINS

Evaluating the return on investment (ROI) is essential to justify the implementation of robotics technology. Assessing the potential productivity gains, cost savings, and increased efficiency resulting from robot deployment helps determine the economic viability of the investment.

 

CONCLUSION

Robotics technology has proven to be versatile and efficient, transforming industries across the globe. With the ability to automate complex processes, increase productivity, and enhance safety, robots have become indispensable in manufacturing, healthcare, logistics, and many other sectors. As the technology continues to advance, the potential for robotics to further revolutionize industries and tasks is limitless. By embracing robotics technology, individuals and businesses can unlock new opportunities for growth, innovation, and success. Selecting the right robot is crucial to ensure optimal performance, safety, and productivity in various applications. Understanding the requirements and considering factors such as payload, reach, end effector compatibility, control capabilities, safety features, and environmental concerns helps make an informed decision. The field of robotics is continuously evolving, with new technologies and innovations being introduced regularly. To gain a deeper understanding and make the best possible decisions, we encourage readers to explore application requirements and product specifications and seek expert advice. Staying updated on the latest developments and engaging with industry experts can provide valuable insights for successful implementation.

 

******

Learn more about how Radwell can support your operation