Posts filed under:
GFM-SYSTEM
BLOG HOME

What is a Gedevelop Camera?

What is a Gedevelop Camera?

A Gedevelop Camera is an air-cooled camera that is designed to withstand heat, smoke, moisture and strong magnetic fields that exist in a fiberizer area. It is used primarily in the manufacturing of insulation. Multiple Gedevelop cameras are connected to a GFM system, which acts as the key component to Glass Flow and Meter measuring.

The Gedevelop camera looks at the glass stream and reads information for stream diameter and stream velocity. The information the camera reads is then sent to the central unit. Based on a set parameter, the glass flow is then calculated. The glass stream is also checked to see if it is at the correct level and if it isn’t, the system adjusts.

Read More

Topics

see all

Signup