Posts filed under:
SERVO-MOTOR
BLOG HOME

The Evolution of the Servo Motor

Servo motors allow for accurate control and precision inside a closed-loop circuit. These motors aren’t necessarily a specific type of motor but rather a combination of certain parts. These devices have been cultivated and improved since the 1800s and have been used in a multitude of different applications. Learn more about what a Servo Motor is here.

Read More

What is a Servo Motor?

A servo motor is a rotary actuator or linear actuator that allows for angular position, acceleration and velocity. It has capabilities that a regular motor doesn’t possess. Servo motors work with sensors for precise control of movement. The controller is the most sophisticated part of the servo motor, as it is designed for precision.

Servo motors are a combination of specific parts, which include a DC or AC motor, and are suitable for use in a closed-loop control system. Servo motor applications include robotics, automated manufacturing and computer numerical control (CNC) machining applications.

The two types of servo motors have different uses. AC Servo motors can handle higher current surges and tend to be used in industrial machinery.

Read More

Topics

see all

Signup