Posts filed under:
PLCS
BLOG HOME

PLCs Power Industrial Data Integration

Not long ago, the roles of industrial automation devices and systems were a little more straightforward. Most field devices and sensors were relatively “dumb” and were directly connected to controllers, which may have interacted with operator displays, and in rare cases some data may have flowed up to higher level enterprise systems. Today’s smart sensors, clever controllers, and more capable communications have improved upon this scenario, and end users are looking for the best ways to enable the enterprise host systems to access valuable field-level data.

Read More

From Crisis to Calm: The Radwell Difference During Crunch Time

It is often during times of crisis in a manufacturing facility that Radwell International is called upon to deliver a solution. Our technicians have spent years honing their skills for exactly the type of situation that occurred with one of our customers this summer.

We received a call at Radwell from one of the manufacturing plants for a large global food manufacturing company. They had called in for an after-hours rush and discovered that Radwell also offered field services which they desperately needed. They were in crisis: their plant was not operational. This was caused by a power surge from one of the utility sub stations, resulting in over 100 drives and other controls and protection devices failing or blowing up due to excessive voltage. This was a major equipment failure situation.

Read More

Industrial Controllers: Past, Present, Future

Since the advent of the programmable logic controller (PLC), automation controllers of all kinds have made their way into industrial applications, including programmable automation controllers (PACs) and today’s edge programmable industrial controllers (EPICs). Users have many options in terms of cost, footprint, input/output (I/O) density, fieldbus compatibility, communication, programming options, and processing speed with competition among vendors looking to establish supremacy.

While it’s generally true diversity is healthy for the market, it also can be a source of frustration for engineers and end users. Selecting a control platform is often a long-term investment and carries related overhead like training and support contracts. Decision-makers want the reassurance they are putting their money to work in the right way.

Read More

Should I Use An Edge Controller, PLC, or PAC?

Edge controllers can provide advantages in many applications where traditional industrial controllers have been used. For commercial and industrial computing products, software and hardware development progress proceeds in tandem, with the lead alternating. Sometimes the software complexity and features increase in a way that bumps into processing limitations; then there are times when hardware advances unleash newfound capacity for more sophisticated software.
It is easy to look at today’s traditional operations technology (OT) industrial controller options, represented most often by traditional programmable logic controllers (PLCs) and process automation controllers (PACs), and see them as mature technologies with capable software and fast hardware. The challenge is identifying what comes next.

A few industry trends are pointing the way. Modern consumer and commercial computing experiences are ripe for merging into industrial products. Internet of Things (IoT) devices are becoming commonplace and many are looking at incorporating Industrial IoT (IIoT) devices into automation systems. Digital transformation requires connecting with many data sources, collecting and storing the data, visualizing and analyzing it, enabling optimized operations.

Read More

Is It Time to Cut the Cable?

The decision to go wireless for machine communication comes down to how much the benefits outweigh the challenges.

 

Wireless communication in our everyday electronic mobile devices has become so pervasive that it’s difficult to remember when such connectivity didn’t exist. Conversely, this level of connectivity has yet to dominate the factory floor. However, with the increased focus on IIoT, this may soon become a reality.

Pneumatic solenoid valves for many decades have been controlled through discrete wiring, with each solenoid individually wired and connected to a common cable, such as a 25-pin D-sub connector. This has progressed to fieldbus for quicker installation times, reduced wiring errors, and more importantly, diagnostic feedback capabilities.

Read More

Optimizing with Automation

Companies today see the potential that exists with automation. When looking towards the optimization of a facility, it is imperative to plan and understand the needs of the operation. Depending on each given business, different automated applications will be best-suited for each respective operation.

Read More

What Is a PLC?

A Programmable Logic Controller (PLC) is an electronic device used to monitor or control production processes. It is a device that a user can program to perform a series or sequence of events. These events are triggered by inputs received at the programmable logic controller through delayed actions such as time delays.

Read More

Strategies for Upgrading PLC Hardware

The programmable logic controller (PLC) first came out in the late 1960s. It's important to know when to update old hardware and controllers with new technology updates and to ensure replacement parts are available in the event of an emergency. 

Key reasons why an upgrade might be necessary include:

 

Read More

Six Questions with Brian Janusz, Global Program Manager at Radwell International

Brian Janusz is an interesting person. He has been central to the redesign and remodel of Radwell International's new headquarters building in Willingboro, NJ. When he wasn't hard at work on managing remodeling and material handling systems,  he has been working with other Radwell locations on expansion plans. Brian is busy: moving frequently and quickly through the 311,000 square foot Radwell headquarters building, easily gravitating from project to project with ease. We caught up with him recently to get a glimspe into his job at Radwell International. We had to walk really quickly to catch up.

Tell us a little bit about yourself and how you came to be at Radwell International.

My education background is in Mechanical Engineering and I graduated from Virginia Tech. My first job out of college was working as a Project Engineer for Bowen Engineering, a great construction company that builds and works on water treatment plants, waste water treatment plants and large utilities. It started off as a summer internship that turned into a full time job. I learned so much from the experience, mostly from the amazing people I worked with. They taught me about project management, people management and construction. It was a difficult job to leave because there was still so much to learn. That experience has helped me enormously, in what I do at Radwell International.

How I came to Radwell: During my freshman year at college I emailed Brian Radwell looking for a summer job. He directed me to Steve Wallace and I got a position helping out in production. That first summer I did anything and everything that was needed. I delivered manual recs, organized the order shelves, cleaned units, worked with speed line testing and approving parts for orders, picked in the warehouse and just generally learned

Read More

Topics

see all

Signup