Posts filed under:
SPEED-CONTROLS
BLOG HOME

Manufacturing Sees Benefits with Machine Vision

Machine vision is making major contributions to the manufacturing sector, primarily by providing automated inspection capabilities as part of quality control procedures. Formerly viewed as barcode readers, these systems now use automated cameras and software to monitor products, collect data, check for inconsistencies, scan labels and perform other functions at high-speeds and without the need for worker intervention.

According to the Automated Imaging Association, machine vision encompasses all industrial and non-industrial applications in which a combination of hardware and software provide operational guidance to devices in the execution of their functions based on the capture and processing of images.

Read More

What Are AC/DC Drives?

AC and DC are different types of voltage or current used for the conduction and transmission of electrical energy.

AC stands for alternating current. AC Drives are frequency converters designed to control the speed and torque of an electric motor. The speed is controlled by changing the frequency of the electrical supply to the motor.

The types of motors that ac drives control normally operate at constant speed. Enabling the user to control the speed of motor potentially gives the user benefits in terms of process control and energy savings.

DC stands for direct current. DC motor drives are a type of amplifier or power modulator that integrate between the controller and a DC motor.

Read More

Topics

see all

Signup